Hi All,
i am seeing a sja1105 driver for linux 4.0 kernel but since our product is based on linux 2.6.35.xx kernel, need this switch over spi there, if any one face this issue, please share the code file either user level/ driver level
Hi shashikant
one can try linux-fslc kernels where it is supported:
GitHub - Freescale/linux-fslc: Linux kernel source tree
GitHub - Freescale/meta-freescale at morty
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Thanks igor,, but we are using ltib as a build rootfs but not yocto, it it was yocto then we would easily get the things move on easily, but this is outdated product with an new eth switch has been integrated , where i am finding difficult to map the driver for LTIB/ which has kernel 2.6.35.abc version. if i get overview of simple application sja1105 code file also fine which shall be able to build on 2.6 linux kernel
any input further.
Hi shashikant
nxp has special service for software customization
Commercial Support and Engineering Services | NXP
Best regards
igor
Thanks igor,, but we are using ltib as a build rootfs but not yocto, it it was yocto then we would easily get the things move on easily, but this is outdated product with an new eth switch has been integrated , where i am finding difficult to map the driver for LTIB/ which has kernel 2.6.35.abc version. if i get overview of simple application sja1105 code file also fine which shall be able to build on 2.6 linux kernel