Hi , I am trying to flash image using the UUU tool.
When flashing an image using the UUU tool, can I use "fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot" in the sample. (I am using sample - L4.19.35_1.1.0_images_MX8MQEVK)
Or should I build "fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot"?
If I try to build with below command, some errors occur.
$bitbake fsl-image-mfgtool-initramfs
Errors are about imx-uuc and imx-kobs.
Solved! Go to Solution.
The fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot is for uuu, you can use the default one, no need to build for it again.
The fsl-image-mfgtool-initramfs-imx_mfgtools.cpio.gz.u-boot is for uuu, you can use the default one, no need to build for it again.
Thanks
Using default one, flash succeeded.
OK