AnsweredAssumed Answered

AP Core TLB not ready on boot (P2020)

Question asked by Alexy Torres on Feb 20, 2020
Latest reply on Feb 25, 2020 by Alexy Torres

Hello,

 

I am writing a bootloader (I cannot use U-Boot in my project) that starts the Core 1 of the P2020 as follows:

1. Copy the Core 1 boot core to 0x00800000 (with branch at 0x00800FFC).

2. Set the BPTR at 0x00800000 (and enable page translation)

3. Release the Core1

 

However, I see while debuging that the Core1 boots correctly to 0x00800FFC, but the TLB is not correct. Indeed it still translates to 0xFFFFF000 -> 0xFFFFF000 for the entry 0.

So Core 1 crashes. 

 

When I update the TLB by hand thanks to the debuger and set the entry 0 to translate: 0x00800000 -> 0x00800000 it works and the Core 1 is able to boot and works perfectly!

 

I am sure I am missing something during the initialization but cannot find it. Do you have any idea on how to debug this?

 

Thanks

Outcomes