Hi Team
We are using iMX 6 solo in one of our custom board, we are able to flash image in SD card through uuu tool using linux, but boards can't able to boot from SD card . Please let us know following
1) During flashing will this iMX internal RAM will be used or external DDR3 will be used ?
2) How we should proceed for debugging this from hardware side ?
Solved! Go to Solution.
Hi Rita
Thanks for replying. We are able to solve the issue basically we were not updating DDR3 setting ,once we updated value obtained from
realview.inc it starts working.
I believe this happens to most of us. I recall I had the same issue a couple of years back. If I'm correct I created a bootable SD card initially. For that, you need to select your SD Card in the Device drop-down menu. The file system should be Fat32.. then check the boxes Quick Format and create a bootable disk. and select FreeDOS for the bootable disk. Press the Start button and wait for it to complete. There you have it. In fact, there are several Chatbot Development Services providers who now create bootable virtual assistant solutions for computers. I believe these are mainly frameworks that help keep files secure and safe and also easily bootable now. Cheers!!
You can check the general troubleshooting steps. You can check with the AI consulting services.
1. Check the SD card
2. Ensure the SD card is compatible with your device and has enough capacity.
3. Verify the SD card is not physically damaged.
4. Use a disk utility to check for errors on the SD card.
5. Reformat the SD card if necessary (be sure to back up any data first).
Is there printing information when your boot up in the serial port?
Hi Rita
Thanks for replying. We are able to solve the issue basically we were not updating DDR3 setting ,once we updated value obtained from
realview.inc it starts working.
Good news, I am very glad it works.
When you boot up your board from SD card, have you set the boot mode to boot up from SD card mode?