1060 API for EMMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1060 API for EMMC

850 Views
sergunionline
Contributor II

Hello dear NXP team

There is now an API for the 1060 board for the EMMC modules with examples.

Thank you

Labels (1)
0 Kudos
2 Replies

777 Views
gredpath
Contributor III

I am trying to use this example on USDHC2, in 8 bit mode so that we can boot from the part. We are testing the hardware of the board, how do I port the example from USDHC1, we have made some changes but I can see nothing on the logic analyser.

Regards

George

0 Kudos

791 Views
FelipeGarcia
NXP Employee
NXP Employee

Hi Sergej,

 

MCUXpresso SDK includes SDMMC drivers and examples in the following path:

 

SDK_2.7.0_EVK-MIMXRT1060.zip\boards\evkmimxrt1060\sdmmc_examples

You can download it from the following link: Welcome | MCUXpresso SDK Builder

 

Best regards,

Felipe

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos