DMA SPI BARE METAL

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DMA SPI BARE METAL

529 Views
hajianik
Senior Contributor I

Hi,

Is there a bare metal example of BARE METAL DMA SPI on S32K14x series available anywhere?

Thanks,

Koorosh Hajiani

Labels (1)
Tags (1)
0 Kudos
1 Reply

434 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Koorosh Hajiani, 

Unfortunately, we don't have any examples that meets these requirements. However, within the cookbook, you will find bare metal examples of SPI and DMA. You could use these examples as a starting point. 

Link to the application note: https://www.nxp.com/docs/en/application-note/AN5413.pdf 

Link to download the software: https://www.nxp.com/webapp/Download?colCode=AN5413SW&docLang=en 

Have a great day,
Victor

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos