10G performance on two LS1046A-RDBs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

10G performance on two LS1046A-RDBs

555 Views
chhsu0229
Contributor II

I have LS1046A-RDM evms to test 10G performance. The two devices are LS1046A-RDBs and run the same LSDK 19.09. The test environment were netperf for test tool, cat6A cable for connect two devs, and all of the setting on these devices were the same. The test results are 1. The average speed (Dev 1 as client and Dev 2 as Server) was 9.89Gps. The result wsa seem correct and closed to 10Gbps. Then, I changed the role, Dev 2 as client and Dev 1 as server and the speed was 7.61Gbps. Why are the result are different on the same device and LSDK? How can I fix these problem?

0 Kudos
1 Reply

462 Views
Pavel
NXP Employee
NXP Employee

Usually is happens if configuration of these boards is different.

 

Perhaps the alien crosstalk happens for your test.

See the following pages:

https://www.belden.com/blog/smart-building/what-you-need-to-know-about-alien-crosstalk-today

 

https://www.datacenterdynamics.com/en/news/cutting-out-the-crosstalk/

 

https://www.csd.uoc.gr/~hy435/material/127_10GBASE_T2.pdf

Have a great day,
Pavel Chubakov

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos