AnsweredAssumed Answered

CLRC663: ISO15693 configuration

Question asked by Akash S on Feb 10, 2020

Hi,

1.

As shown in the above table, ISO15693 supports 10 to 30% ASK or 100% ASK. A higher modulation index would lead to a higher bandwidth and lower range and a lower modulation index would result in low SNR.

How to select the right modulation index for an application?

 

2. How to configure 100% modulation index as the Table 32 of datasheet shows configuration bits for 0.5 to 60% only?

 

3. Does the data rate have an impact on the range?

Outcomes