AnsweredAssumed Answered

iMXRT1064 with external Flash as non XIP

Question asked by Anuj Tanksali on Feb 10, 2020
Latest reply on Mar 6, 2020 by Anuj Tanksali

Hello,

 

I am using iMXRT1064 controller with Emwin graphical library. I have a lot of images in my application so wanted to use an external flash for storing the images. 

 

Is there any facility in iMXRT1064 device which can directly access serial flash as non XIP.

My code will execute from internal flash and access the external flash for images. 

 

I do not want to build a separate binary file for images which i will have to program it in external flash first then i can access the images from internal flash through code in internal flash

 

Is it possible using iMXRT1064? 

If yes then is there any example for it?

 

Regards,

 

Anuj

Outcomes