AnsweredAssumed Answered

DDR Validation using Codewarrior Debug ls1021a standalone

Question asked by Elias Bitbaker on Feb 9, 2020
Latest reply on Feb 18, 2020 by Yiping Wang

Hi,

 

I have a customized ls1021a, an external SD card breakout which I hard strap the cfg source pins to the SD as the boot source. I could not detect any activity from my serial console which was connecting the UART1 (default serial pins by the uboot) from the CPU to the FTDI interface.

 

So then I performed a debug using Codewarrior. I am able to establish the communication between the CPU and the codewarrior via JTAG interface.

 

 

But the thing is how do I know if the internal ROM instructs the DDR to copy some of the image into the DDR from the boot source (SD card). What is the address in the memory mapping to save those data of the SD card so that I can ensure the image is copied to the DDR.

 

(edited)

(2) I have the access into the my board now from serial console but it shows 1 GB of DDR but I have 4 GB DDR what is the issue here ?

Outcomes