Hello,
My question is: how to send IMSG traces to uart4?
In details:
- I work with an i.MX 8M Mini EVK board (machine imx8mm)
- I have built an image (full-command-line) from imx-linuxwarrior (imx-4.19.35-1.1.0)
- Boot is OK, testx is OK
- I can build and run optee demo samples BUT no way to see IMSG text.
I build TA with CFG_TEE_TA_LOG_LEVEL ?= 4
I checked in "conf.mak" that trace is enabled: CFG_TEE_CORE_TA_TRACE=y
In this file I see also that CFG_UART_BASE=UART2_BASE
- is it the right value?
- if not, where to change this value to be compiled with (i see this value in many .mk files...)
In another file "build/tmp/work-shared/imx8mmevk/kernel-source/arch/arm64/boot/dts/freescale/fsl-imx8mm-m4.dts"
I tried to change the status of uart4:
&uart4 {
status = "okay";
};
but no change, uart4 is still silent.
Thanks in advance for your help.
Best Regards
Ronan
Hi Ronan
one can try solution suggested on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------