Help with PN7150 code examples for P2P uri transfer C# preferred

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Help with PN7150 code examples for P2P uri transfer C# preferred

791 Views
subscribe
Contributor I

Hi there community I am fresh to the NXP community so go easy...

I recently purchased a PN7150 with the intention of writing an app that would simple send a uri via ndef from a windows device to another NFC enable device. I hope to use visual studio, the issue is that the supplied sample code for this device is very difficult to interpret, the code appears to enable all functions of the device and is difficult to follow.

Can anyone point me to c++ c# examples of code of how to achieve this task or any other demos, showing P2P transfer of uri from a device to another

0 Kudos
1 Reply

720 Views
nxf58474
NXP Employee
NXP Employee

Hi,

 

Sorry for the inconveniences this might cause you but we do not have an example for visual studio per your requirement.

 

The closest element that we have available will be the some of the linux examples we have available for the different options of kit that you can find in this page under the software tab.


Something that I would like to clear up and confirm is that the PN7150 works command based so it needs a host to send the commands through I2C .

 

Hope this helps .

 

Best Regards,

Ricardo

0 Kudos