Hi
Please let me make clear about below two questions.
〇Question about ①
・Does this mean;
a)Supplied voltage for all IO group(NVCC_xxx) must be the same voltage?
b)Supplied voltage is depends on application requirement, but need to apply voltage at the same timing?
・Any requirement about supplied voltage timing?
〇Question about ②
・This path(from NVCC_LVDS_2P5 to DRAM_IO/RGMII_IO) can be on/off by register setting?
Br,
Yuji
Hi, Igor
>what processor used in the case ?
Using I.MX6 Dual Lite.
>a). NVCC_xxx can be different.
I understood different voltage can be applied to each NVCC_xxx.
> b). timings can be found in Datasheet, "Power Up Sequence" chapter.
Yes, i know the below chapter on the datasheet, but no mentioned about NVCC_xxxx timing.
Where should I refer to understand more detail requirement about it?
>voltages which can be turned off are given in Hardware Guide, in sect."Unused Peripherls".
Which Hardware guide should i refer to?
I checked below notes, but i was not able to find that sect.
|Common Hardware Design for i.MX 6Dual/6Quad and i.MX 6Solo/6DualLite
|Hardware Development Guide for i.MX 6QuadPlus, 6Quad, 6DualPlus, 6Dual, 6DualLite, 6Solo Families of
Applications Processors
Br,
Yuji
1, NVCC_xxxx can be applied after VDD_SNVS_IN
sect.2.8 Unused analog interfaces
Best regards
igor
Hi Yuji
what processor used in the case ?
1. a). NVCC_xxx can be different.
b). timings can be found in Datasheet, "Power Up Sequence" chapter.
2. voltages which can be turned off are given in Hardware Guide, in sect."Unused Peripherls".
All other voltages can not be turned off.
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------