Hi,
I am trying to configure OV5640 ( MINISASTOCSI) with the imx8mq EVM with one lane config. I followed the process as described in Single Lane Mipi interface to i.mx6
However, the camera did not stream any data with the following command:
gst-launch-1.0 v4l2src device=/dev/video0 ! video/x-raw,width=640,height=480 ! autovideosink
The same command works with the default 2 lane config.
I suspect the clock requirements on the DPHY side is not met.
Do we have any pointers on how to debug this for imx8. Most of the documentation available is for i.mx6 or 7.
I also changed the clock to as follows:
drivers/clk/imx/clk-imx8mq.c
clk_set_parent(clks[IMX8MQ_CLK_CSI2_CORE], clks[IMX8MQ_SYS1_PLL_800M]);
However, the camera still failed to stream.
Hi Subhasish
for one lane configuration one can look at
https://community.nxp.com/thread/498568
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------