How to program GPIO pins to accept a signal from the signal generator and sample it using HSADC of LPC-Link2 board(LPC 4370) in LPCXpresso

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to program GPIO pins to accept a signal from the signal generator and sample it using HSADC of LPC-Link2 board(LPC 4370) in LPCXpresso

777 Views
naveen_b160496e
Contributor I

Also, can I get the program for configuring the GPIO pins as input and output of LPC-Link2 board with LPC 4370 microcontroller. 

0 Kudos
2 Replies

699 Views
bernhardfink
NXP Employee
NXP Employee

Maybe you find examples in the attached package.

Regards,

Bernhard.

0 Kudos

699 Views
xiangjun_rong
NXP TechSupport
NXP TechSupport

Hi, Naveen,

This is the figure the ADCHS analog input pins, as you can see that the ADCHS analog input pins are independent analog pins, they are not multiplexed with the GPIO or any other peripherals, so you do not need to configure anything for the ADCHS analog pins.

Mr Bernhard has attached the example package,pls check it.

BR

XiangJun rong

pastedImage_1.png