Hello,
I am using RT1020 to connect to a switch via RMII interface.
The reference clock is provided by the switch.
and I am using the SDK sample code
lwip_tcpecho_freertos
Do I only need to make modification to change the ENET_TXCLK direction to input?
Hello Benson,
In RMII mode ENET_REF_CLK signal is the reference clock for receive, transmit, and the control interface. According to Table 36-2 of the reference manual, this pin by default is set as an input.
Have a great day,
Victor
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------