Encrypt XIP: What is "SW pin on your board to enable XIP"?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Encrypt XIP: What is "SW pin on your board to enable XIP"?

1,151 Views
rshipman
Contributor V

Document: AN12079.pdf: How to use i.MXRT Security Boot, Application Notes, Rev. 0, 10/2017

Section: 3.3.3. Download the image

Pages: 27

What does the author mean by the words:

"At last set the SW pin on your board to enable XIP and run the application. Remember to reset the SW pin selection to change the boot mode and enable XIP, then you can reset and run."


What is the SW pin selection? Do they mean the boot config DIP switches?

Why set and then reset to enable XIP?

Labels (2)
Tags (1)
0 Kudos
5 Replies

1,048 Views
rshipman
Contributor V

I looked at the schematic for the RT1020-EVK.

Dip switch SW8-1 controls the EncryptedXIP fuse bit (BOOT_CFG[0]) via GPIO_EMC_18 (I guess because the fuse isn't locked).

However it is not clear what the boot settings should be when EncryptedXIP is on. I presume set them for internal boot (or from fuses if these are set up correctly)?

0 Kudos

1,048 Views
rshipman
Contributor V

And the RT1050-EVKB uses SW5-1. This DIP switch is not fitted so you have to solder on your own or close the circuit in some other way during boot.

Encrypted XIP works ok on the RT1050-EVK, using SW5-1.

I have not yet managed to get Encrypted XIP to work on the RT1020-EVK.

0 Kudos

1,048 Views
Yuri
NXP Employee
NXP Employee

Hello,

 

  You are right, the SW pin relates to Boot Mode Configurations, based on board switches.

Switch (SW7-3 & SW7-4) is used to select the boot mode on the MIMXRT1050 EVK Board.

Use sheet 16 of the EVK (.pdf) scheme for more details.

 

https://www.nxp.com/webapp/Download?colCode=MIMXRT1050-EVK-DESIGNFILES-A1&appType=license 

 

 For i.MX RT1020 EVK, use sheet 14 of the EVK (.pdf) scheme for more details.

 

https://www.nxp.com/webapp/Download?colCode=MIMXRT1020-EVK-Design-Files 

 

  Note, different boot modes are applied for the Serial Downloader and the XIP.

 

  To apply the MFG tool BOOT_MODE[1:0] = 01 (Serial Downloader mode) should

be used. And BOOT_MODE[1:0] = 10 (Internal Boot mode) should be used for the XIP.

 

Have a great day,

Yuri.

 

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored

 

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

0 Kudos

1,048 Views
rshipman
Contributor V

Encrypted XIP works on the RT1020-EVK and the RT1050-EVKB.

0 Kudos

823 Views
navoda
Contributor II

Hi @rshipman ,

 

Can you please briefly explain the steps you took to get an encrypted XIP image running on RT1020-EVK?
I did the following steps and it didn't run.

- Generated a bootable XIP image from MCUXpresso IDE with XIP_BOOT_HEADER_ENABLE=0 (iled_blinky)
- Encrypted the image using the Secure Provisioning Tool
- Set BEE_KEY_SEL0 fuse to SW-GP2
- Burnt the user key to SW-GP2
- Set  the EncryptedXIP bit to 1
- Programmed the board
- Tried with DIP switch set to both configurations: 0010 and 1010. Neither of them worked.

0 Kudos