AnsweredAssumed Answered

How to use more than one application of IOT toolbox in one code?

Question asked by Chintan Patel on Jan 31, 2020
Latest reply on Feb 27, 2020 by Mario Ignacio Castaneda Lopez

Hello,

 

I am new in development with NXP KW36 module. My requirement is to create one project which have below functionalities:

   1. wireless uart

   2. Over the air programming for upgrade image.

I have go through the example codes of Wireless uart and OTAP, to know the how codes work.

I have tested both codes with NXP IOT application, and they are working fine individually.

 

I am using NXP IOT application. As each example has different UUID, I can see the module in that specific demo in NXP IOT application. So, when I upload the image file of wireless uart project via OTAP, in IOT application it will show only in the Wireless uart demo. I will not able to see my module into OTAP demo.

 

What changes I have to do in my project, so I can see my advertising KW36 module in both Wireless uart and OTAP demo of IOT application?

Can I add both UUID128 of wiress uart and OTAP, in one file?

How can I merge two applications' code into one project?

 

The reason of doing this as I want to upload my project via OTAP again after making changes into it.

 

Kindly guide as I am stuck in my project and it's urgent.

 

Information:

Example code: frdmkw36_wireless_examples_bluetooth_w_uart_bm

Development module: FRDM KW36

 

Thank you.

Outcomes