AnsweredAssumed Answered

i.MX RT1064 & Internal 4MB of Flash   

Question asked by Atzel Collazo Employee on Jan 29, 2020
Latest reply on Jul 9, 2020 by Sabina Bruce

Hello team,

 

I'm trying to figure out how the internal 4MB of Flash in the RT1064 works, I want to recommend the device to a customer looking for an MCU with the amount of RAM that RT has and the power of processing.

I'm not being able to understand how it works. From the RM I understand that it must be accessed using the FlexSPI but I don't know if it can be used as a regular flash to store the program/application and run from there. is it possible? if so, is it ECC protected?

 

Thanks!

Best Regards,

Atzel Collazo

Outcomes