AnsweredAssumed Answered

iMXRT Camera Cmos

Question asked by Rubens Junior on Jan 27, 2020
Latest reply on Jan 31, 2020 by Felipe García

Dear collegues!

 

I need to integrate the NXP processor with a CMOS camera that is not between the OV7725 and MT9M114 models. In the NKP SDK's and documentation, only these two CMOS models are supported. However, I will use CMOS GC0308 in my project, for which I need yours guidance to establish communication with the iMXRT1051 processor. I basically need to capture a static image.

 

Thanks a lot!

Best regards!

 

Rubens Júnior

Outcomes