AnsweredAssumed Answered

MPC5566 BAM eSCI serial configuration

Question asked by Ryan K on Jan 24, 2020
Latest reply on Jan 27, 2020 by Ryan K

I'm just starting to utilize the BAM through eSCI. Starting with the password exchange at the beginning, I tried to use the serial configuration specified in the manual (section 16.3.2.3.2) which is "one start bit, eight data bits, no parity and one stop bit". When I send the password, a response comes back but my serial terminal drops one of the bytes. If I change my config to have odd parity instead of no parity, then I receive the full password back correctly.

 

Is this an error in the reference manual?

Outcomes