Hi sir,
I am working on KIT33771TPLEVB(slave board), S32k144 EVB(master) and KITMC33664 (Interface board between master and slave to convert SPI to ISO-SPI and vice versa). using TPL (iso-spi) communication, i am trying build communication between master and slave. SPI data is transmitted from master board. i am not sure data is going into slave or not. can anybody help how can i wake up the KIT33771TPLEVB(slave board) using TPL communication.
Regards,
Veeraju V Hallikeri#
Hi Veeraju,
Please take a closer look at our complex BCC Package including the SW driver, UM11143 with evaluation boards settings and example projects for S32K144EVB-Q100.
You can download it from:
In addition to that, there is the AN12084 (MC33771B/MC33772B Programming Guide) providing basic guidelines for configuration and programming of the MC3377x.
However, it is currently available for download from DocStore under NDA (Non-Disclosure Agreement) only:
Hope it helps!
Best regards,
Tomas