Unidentified LS1020 personality (DCFG_CCSR_SVR)

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unidentified LS1020 personality (DCFG_CCSR_SVR)

622 Views
lucroy
Contributor III

We have LS1020 ICs  which have undocumented personality (DCFG_CCSR_SVR [VAR_PER]) in ls1021 reference manual rev3.

We get the following:

0x87081320

 

MFR_ID 8
SOC_DEV_ID 70
VAR_PER 813 1000 0001 0011
MAJOR_REV 2
MINOR_REV 0

 

Can you tell us the nature of the unlisted personality (VAR_PER)?

Tags (2)
0 Kudos
1 Reply

559 Views
alexander_yakov
NXP Employee
NXP Employee

Sorry for delay.

Please check pins IFC_A16 and IFC_A17

 

LS1020A datasheet,  Table 1, note #5 bellow the table states the following: 

 

  1. Pin must NOT be pulled down during power-on reset. This pin may be pulled up, driven high, or if there are any externally connected devices, left in tristate. If this pin is connected to a device that pulls down during reset, an external pull-up is required to drive this pin to a safe state during reset.
0 Kudos