How to read Multiple ICODE ILT tags using clEV6630B board ? (CLRC663 plus transponder)
I have tried the advance discovery loop evaluation example by changing the MAX_DEVICE_LIMIT to 50. But it is able to read only up to 8-10 tags even though 30+ tags in the field.
1. What is the maximum possible number of ICODE ILT tags we can inventorize using CLEV6630B board ? The idea is to read
50+ tags.
2. If the answer to the maximum possible number to the above question is more than 10, what software changes required in the
Advancdiscovery loop example to inventorize 50+ tags.
#ICODE ILT
Hello,
Currently the NXP NFC Reader Library also implements the Type-V anticollision. If you follow the path of the Discovery Loop you will end up at the anticollision function for Type-V in a file called 'phacDiscLoop_SW_Int_V.c', the method 'phacDiscLoop_Sw_Int_CollisionResolutionV(...)' implements the anticollision.
Regards,
Estephania