QN9080: How to adjust tx power on HCI.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

QN9080: How to adjust tx power on HCI.

996 Views
danieltseng
Contributor V

I study HCI program. I want to adjust tx power on HCI.

The annotation of "Controller_SetTxPowerLevel()"  understand that it only supports kw40 and kw41.

pastedImage_1.png

The following "20" should be about the value range of KW41, not QN9080

pastedImage_2.png

I found the following functions that are related to QN9080

pastedImage_3.png

I tried to enable it, but it didn't work (always gray)

pastedImage_6.png

The following is the adjustment value of qn9080, which is different from 0 ~ 32 of kw41 above.

pastedImage_5.png

My questions are as follows

1。Is tx power currently under program control? Or go to the preset 0x7F

2。Is the QN9080 program for adjusting tx power available?
3。How can I adjust tx power by program?

Labels (1)
  • QN

0 Kudos
2 Replies

897 Views
renatozapatalus
Contributor I

Hello Estephania! 

I've tried the tutorial in the link you provided (Custom HCI command), although it didn't work because the fsl_xcvr.h does not exist in my project. I searched in the SDK files, but I couldn't find it.

I'm using a QN9080-001-M17, does the fsl_xcvr.h exists for QN?

I'm trying to change the advertising tx power in the wireless uart project, is it possible?

Regards,

Renato

0 Kudos

897 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

Could you please help me check this other post ?

https://community.nxp.com/docs/DOC-341764 

Regards,

Estephania

0 Kudos