I have CW10.6, and need to modify a "WL" package (28 pin SOIC). The only options in CW are for a LC or FM.
If I need to upgrade or pay a new license, I will.
Any help will be greatly appreciated.
I checked CW10.6, It can support 9S08QE8CWL, see attached video.
Have a great day,
Jun Zhang
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------