AnsweredAssumed Answered

S32K144 I2C pins are don't work

Question asked by Minsik Choi on Jan 16, 2020
Latest reply on Jan 17, 2020 by Daniel Martynek

I was going to take a [Example_S32K144_I2C_Master_MPL3115A2_S32DSR1_v3] file and test the I2C communication with this project. Both the SDA and SCL should be high (5 V) in IDLE state, but pins PORTA2, PORTA3, were measured with the oscilloscope, both of which produced low (0 V) output. The slave was not connected. What's wrong with the project or the board?

Outcomes