AnsweredAssumed Answered

adb devices not detecting device

Question asked by Srinivas Jakkula on Jan 15, 2020
Latest reply on Jan 15, 2020 by Wigros Sun

Hi,

 

I have installed Windows 10 on Virtualbox on a MAC host.

Installed android platform-tools and tools and updated the environment variables.

After this, I have connected the Indigo2 device (imx8mn nano) to the system

Then connected USB device to Windows machine from the menu (Devices  -> USB -> Jupiter USB device) as shown in the IMG-5037.jpg

Then opened the Device Manager in the Windows (Virtual system). Scan for new hardwarde as shown in IMG-5038.jpg

 

Here the device is shown. But adb devices is not recognizing the device

 

After this, I have tried to update the  driver using using ADB device driver and also WinUsb Device Driver as shown in IMG-5040.

 

In both cases, I am getting error as "This device cannot start (Code 10) Error.

 

Any help is appreciated as I am using this for first time on a fresh installation of Windows 10

 

Let me know if any other information is needed. I am able to connect to serial console to that same Windows machine for console logs

 

/Srini

Attachments

Outcomes