I am using NXP K60 processor now it is interfaced with 16MB (4KB Sector Erase N25Q128A) external SPI flash . i am planning to update the flash size up to 64MB (4KB, 32KB, 64KB, Sector Erase MT25QL512ABB) is need any SPI driver modifications?
Hi,
I am so glad to serve you.
As you mentioned, the flash has been updated to 64MB, and the first point is change the "#define flash_size xxxx".And there may has some other cmd ,you can add the cmd to the head file for useing. And new cmd could be packed into a new fuction. For more difference,please refer to the RM and datasheet.
Jianyu:
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------