Hi,
Please can i know how to dump the register values of wm8960.since I'm facing issue with audio when aplay is used.
Hi Dhanush
if codec is connected via i2c, one can try to read its registers using i2c tools:
https://community.nxp.com/docs/DOC-343682
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igor,
thanks for your reply.
Im stuck at one position from many days,Please can you help me to resolve
the issue.
During the porting of wm8960 codec , Im facing the issue like there is no
clk signals(BCLK,FCLK,Tx) ,except mclk from processor.
Tool chain -- Yocto
BSP -- 4.9.11
Processor -- IMX6UL
Interfaces -- i2c1,sai2
dts interface: