How to solve this problem? Does the flash scrubbing have to do with it?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to solve this problem? Does the flash scrubbing have to do with it?

383 Views
1010663655
Contributor I

We have one piece of MCU which type is SPC5748, after we have burned different programs with the Multilink Universal for it several times, we can never program successfully and it would be dying at Verifing(as shown below). How to solve this problem? Does the flash scrubbing have to do with it?

Connection from "127.0.0.1" via 127.0.0.1

Copyright 2017 P&E Microcomputer Systems,Inc.

Command Line :C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\pegdbserver_power_console -device=MPC5748G -startserver -singlesession -serverport=7224 -gdbmiport=6224 -interface=USBMULTILINK -speed=5000 -?

 

CMD>RE

 

Initializing.

MPC574xC Device detected.

Target has been RESET and is active.

CMD>CM C:\NXP\S32DS_Power_v2017.R1\eclipse\plugins\com.pemicro.debug.gdbjtag.ppc_1.7.2.201709281658\win32\gdi\P&E\nxp_mpc5748g_1x32x1520k_cflash.pcp

 

Initializing.

MPC574xC Device detected.

Initialized.

 

;version 1.05, 06/26/2017, Copyright P&E Microcomputer Systems, www.pemicro.com [5748G_6080k]

 

;device NXP, MPC5748G, 1x32x1520k, desc=CFlash

 

;begin_cs device=$00F90000, length=$005F0000, ram=$40000000

 

Loading programming algorithm ...

 

WARNING - Selected .PCP file has been modified. CRC16 = $5A63

Done.

CMD>VC

Verifying object file CRC-16 to device ranges ...

   block 00FA0000-00FA0003 ...

0 Kudos
0 Replies