Passthrough of SPI devices on NXP iMX8QM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Passthrough of SPI devices on NXP iMX8QM

584 Views
kasandesh
Contributor II
Hello All,
From the documentation, what i understood is, for the passthrough Dom0 doesn't have any influence. The drivers of peripherals that has been passthrough has to be enabled in the guest domain.
With this understanding, i have created the partial-device-tree.dtb and configuration file for the SPI passthrough device on XEN for iMX8QM target.
Both the files have been attached. But the SPI devices are not seen in guest domain.
It would be of great help, if someone could point me where i am going wrong.
Thanks in advance,
0 Kudos
1 Reply

504 Views
igorpadykov
NXP Employee
NXP Employee

Hi Sandesh

I am afraid passthrough is not supported in nxp bsps, in general one can look

at documentation example :

passthrough.txt\arm\misc\docs - imx-xen - i.MX Xen 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos