AnsweredAssumed Answered

Secure Element SE050 with freertos.

Question asked by jb@altaneos.com on Jan 8, 2020
Latest reply on Jan 13, 2020 by Estephania Martinez

Hello,

 

I'm trying to use the SE050 (with the board OM-SE050ARD) on a esp32 without Cmake.

 

I succeeded with a Linux board (with Cmake and the quick start guide) but I'm blocked with esp-idf (v4.0 beta1).

I can't add the plug and trust middleware to my project. I'm following the middleware porting guide without any success.

Do you know if there is an "only MCU" version with only the library I've to had to the project? Because I can't find the file I had to include or not. 

 

My objective is to implement the SE050 certificate verification in mbedtls.

 

Thank you

Outcomes