AnsweredAssumed Answered

EXT_CHANNEL_23 in S32K146

Question asked by BJ RAJENDRANATH on Jan 7, 2020
Latest reply on Jan 7, 2020 by BJ RAJENDRANATH

Hi,

 

I'm trying to use S32K146 module & standard SDK_GCC in order to use ADC module.

 

As the S32K_RM suggests S32K146 -144LQFP supports ADC with 24 channels which can be selected using ADCSCR register.

 

 

 But in the adc module which I selected from the library is not showing EXT_CHANNEL _23 instead it shows only till EXT_CHANNEL_15.

 

Also I observed that it takes CPU with 100 pin but I couln't able to see how can I modify to 144 pin

 

Kindly help in this regard.

 

Raju

Outcomes