AnsweredAssumed Answered

EglCreateDisplay fails with new vivante 6.2.4 p2.3 drivers

Question asked by Nico Coesel on Jan 3, 2020
Latest reply on Jan 9, 2020 by Bio_TICFSL

Hello,

I have upgraded to a newer version of the Vivante drivers from p1.8 to p2.3. I can compile & link my application just fine but now EglCreateDisplay fails on a Wayland screen. What I see is that in the new driver package there is a libEGL.so.1.0 which is linked to by libEGL.so.1 . In the p1.8 version libEGL.so.1.0 didn't exist and libEGL.so.1 linked to a wl (wayland) specific version of the library. With the p2.3 version the generic library is used instead of the ones in the wl directory. The same goes for libGLESv2. Is there a fix for this?

 

The Weston GUI environment works just fine BTW.

 

Thanks in advance.

Outcomes