Hello:
I have a lx2160ardb board,and i want to use code warrior to download uboot,rcw... to boot the board,but i have someproblem in use code warrior, In document, CodeWarrior Development Studio for
QorIQ LS series - ARM V8 ISA, Targeting Manual , on 2.2 CodeWarrior Executable Importer wizard ,iwant to select the type of u-boot, but ,it did not work, i can't select any type, can someone help to fix this ,thanks!
Hello zhengling liu,
You need to create a bareboard project to connect to the target board to do flash programming.
For bareboard project creation, please refer to the section "3.2 Working with bareboard application" in C:\Freescale\CW4NET_v2019.01\CW_ARMv8\ARMv8\Help\Getting_Started_for_CW_ARMv8.pdf.
For flash programming, please refer to the section "1. CodeWarrior Connects to the Bare Board to do Flash Programing" in https://community.nxp.com/docs/DOC-331981.
Thanks,
Yiping