imx6solo-overlay问题

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imx6solo-overlay问题

440 Views
dengguozhen
Contributor I

The superposition shows two pictures a and b in the same fb, picture a is on the top and picture b is below. Every time the first display is started up, picture a superimposed on the surface must lose some pixels when displayed, and then it will display normally. What is the problem?With ipu

Labels (1)
0 Kudos
1 Reply

405 Views
igorpadykov
NXP Employee
NXP Employee

Hi guozhen

such case is decribed in sect.7.3.1.6.3 Multiple videos overlay Linux Guide

included in Linux 4.19.35_1.1.0 Documentation

So one can try it.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos