Are there UART0_TX and UART0_RX pined out in LPC11U68Xpresso?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Are there UART0_TX and UART0_RX pined out in LPC11U68Xpresso?

1,015 Views
fjrg76
Contributor IV

This is the first time I've tried to use the DEBUGSTR() (and associated functions) utility provided in such board. However, it seems that the PIO0_18 and PIO0_19 pins ARE NOT pinned out to any of the several board's connectors.

What am I missing?

Labels (2)
0 Kudos
1 Reply

844 Views
fjrg76
Contributor IV

I found the answer. Such pins aren't pinned out; instead, they are connected directly to the LPC4322 chip (the one that serves for debugging) so we can use the USB port for the UART. It means we don't need either the pins pinned out nor a TTL-USB adapter, awesome!

I documented my discovery in my blog in case you're interested in the topic.

Thank you!!!