Is is possible to use the ADC interrupt for multiple ADC channels which have different operations?

Discussion created by Guest on Mar 23, 2009
Latest reply on Mar 23, 2009 by bigmac

Hi. I'm currently working on the ADC interrupt. It seems to me that I can only use it for one ADC channel. I would like to know if I can use the interrupt for different channels. For example, I would like to use ADC channels AD1 and AD5, both having different operations when interrupted. Can I assign a unique interrupt to each of them?

 

I'm using MC9S08AW60 MCU, which only has one vector number for the ADC interrupt. Thx  

Outcomes