I have noticed that when I set up a project in the MCUXpresso for the LPC55S66, the name of the startup file is called startup_lpc55s66_cm33_core0.c.
Similarly, when I start a project for the LPC55S66 in IAR, it asks me to choose between core 0 and core 1.
What is the difference?
Bob N
Thanks, Jeremy.
Is there an SDK example project that uses both cores?
Bob N
Hi Bob Nayar,
Thanks for your reply.
1) Is there an SDK example project that uses both cores?
-- Please refer to the multicore_examples in the SDK library.
Have a great day.
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi Bob Nayar,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) What is the difference?\
-- The LPC55S6x/LPC55S2x/LPC552x device is the dual-Cortex M33 core MCU, it allows the demo project to be executed in either core 0 or core 1.
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------