AnsweredAssumed Answered

S32K146

Question asked by WANG LI on Dec 24, 2019
Latest reply on Jan 5, 2020 by Daniel Martynek
  • S32K148 code is normal runing.
  • Port S32K148 code to S32K146报错如下:

 

  freeRTOSconfig.h

-#define configTOTAL_HEAP_SIZE                    ( ( size_t ) 98304 )

+#define configTOTAL_HEAP_SIZE                    ( ( size_t ) 30*1024)

 

  • The compile passes, but the program does not execute within the task.

and use JLINK DEBUG:

 

ERROR: Can not read register 44 (FPS11) while CPU is running
ERROR: Can not read register 45 (FPS12) while CPU is running
ERROR: Can not read register 46 (FPS13) while CPU is running
Read 4 bytes @ address 0xDEADBEEE (Data = 0x00000000)
WARNING: Failed to read memory @ address 0xDEADBEEF
Removing breakpoint @ address 0x000011F4, Size = 2
WARNING: Failed to read memory @ address 0xDEADBEEE

 

thanks

Outcomes