SDHCI REGISTER DUMP in i.mx8mmini

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SDHCI REGISTER DUMP in i.mx8mmini

860 Views
santhosh2
Contributor IV

Hi,

I have implemented Watch dog timer and configured at 1min and resetting the WDT at every 5 seconds.  The processor was in the below error state for more than 5 min before it could restart itself. I have no clue about this error help me to find the root cause of this below error (Log file is attached for quick info)

[107434.234408] mmc0: Timeout waiting for hardware interrupt.
[107434.239900] mmc0: sdhci: ============ SDHCI REGISTER DUMP ===========
[107434.246428] mmc0: sdhci: Sys addr:  0xbbbde51c | Version:  0x00000002
[107434.252955] mmc0: sdhci: Blk size:  0x00000004 | Blk cnt:  0x00000001
[107434.259481] mmc0: sdhci: Argument:  0x9410d004 | Trn mode: 0x00000003
[107434.266008] mmc0: sdhci: Present:   0x01d88008 | Host ctl: 0x00000013
[107434.272534] mmc0: sdhci: Power:     0x00000002 | Blk gap:  0x00000080
[107434.279060] mmc0: sdhci: Wake-up:   0x00000008 | Clock:    0x0000001f
[107434.285587] mmc0: sdhci: Timeout:   0x0000008f | Int stat: 0x00000103
[107434.292112] mmc0: sdhci: Int enab:  0x107f110b | Sig enab: 0x107f110b
[107434.298639] mmc0: sdhci: AC12 err:  0x00000000 | Slot int: 0x00000502
[107434.305165] mmc0: sdhci: Caps:      0x07eb0000 | Caps_1:   0x8000b407
[107434.311690] mmc0: sdhci: Cmd:       0x0000353a | Max curr: 0x00ffffff
[107434.318217] mmc0: sdhci: Resp[0]:   0x00001000 | Resp[1]:  0x00000000
[107434.324744] mmc0: sdhci: Resp[2]:   0x00000000 | Resp[3]:  0x00000000
[107434.331268] mmc0: sdhci: Host ctl2: 0x00000088
[107434.335798] mmc0: sdhci: ADMA Err:  0x00000000 | ADMA Ptr: 0x78089208
[107434.342323] mmc0: sdhci: ============================================
[107434.349298] AR6000: SDIO bus operation failed! MMC stack returned : -110
[107434.356191] __HIFReadWrite, addr:0X000868, len:00000004, Write, Sync

Regards

Santhosh Kumar S

0 Kudos
4 Replies

681 Views
jimmychan
NXP TechSupport
NXP TechSupport

could you tell me which version of BSP are you using?

0 Kudos

681 Views
santhosh2
Contributor IV

Version.png

Linux Version is 4.14.78_1.0.0

0 Kudos

681 Views
jimmychan
NXP TechSupport
NXP TechSupport

Is the SDHC connecting to a device called AR6000? You may try to add some printf in the driver to see where it stop?

0 Kudos

681 Views
santhosh2
Contributor IV

I have no idea where to add.. Can you guide which file to touch

Regards

Santhosh

0 Kudos