AnsweredAssumed Answered

S32DS_Power_Linux_v2.1 installer fails on Ubuntu 18.04

Question asked by Jed F on Dec 15, 2019
Latest reply on Dec 17, 2019 by Jed F

The S32DS Power installer for Linux is failing on my Ubunt 18.04 machine.

$ ./S32DS_Power_Linux_v2.1.bin
Preparing to install
Extracting the installation resources from the installer archive...
Configuring the installer for this system's environment...

Launching installer...

An internal LaunchAnywhere application error has occured and this application cannot proceed. (LAX)

Stack Trace:
java.lang.IllegalArgumentException: Malformed \uxxxx encoding.
    at java.util.Properties.loadConvert(Properties.java:574)
    at java.util.Properties.load0(Properties.java:391)
    at java.util.Properties.load(Properties.java:317)
    at com.zerog.common.java.util.PropertiesUtil.loadProperties(Unknown Source)
    at com.zerog.lax.LAX.<init>(Unknown Source)
    at com.zerog.lax.LAX.main(Unknown Source)

I downloaded it multiple times and all have the same checksum sum:

8a1fbf7f9ddf85dae1e0b8ce43aef83da5a347ba4ff7bdddd66b061ddf468b77  S32DS_Power_Linux_v2.1(1).bin
8a1fbf7f9ddf85dae1e0b8ce43aef83da5a347ba4ff7bdddd66b061ddf468b77  S32DS_Power_Linux_v2.1.bin
8a1fbf7f9ddf85dae1e0b8ce43aef83da5a347ba4ff7bdddd66b061ddf468b77  S32DS_Power_Linux_v2.1.bin?ftpRequestID=7484059977&server=freescaleesd.flexnetoperations.com&dtm=DTM20191215141940Nzk2MTc3NjU0&authparam=1576448380_fadfa4d53bb2515129868cb9772f67b0&ext=.bin

 

Which raises more issues:

 

1. Can you just release the GCC binaries separate? I have no desire to ever use the IDE.

2. Why is NXP so bad at opensource? I realize the PowerArchitecture skews to automotive, but just dumping a bunch of patch files on the community is absolutely not what opensource is about.

3. platformio support would be amazing. But I know that's a pipe dream.

Outcomes