Hello community,
If default Linux BSP image, it have H/W VPU library and enable VPU module clock and power,
on no-VPU device like MCIMX6Q4AVT08AER, what happen to run video encode/decode application
on this device?
On this device, it can call software video enc/dec library automatically?
Or to use no-VPU device, does it must need to use some special kernel
disabled VPU expressly?
Best regards,
Ishii.
Solved! Go to Solution.
No, you don´t need re-configured, Uboot detect which processor do you have, and the VPU is disable.
Hello Takayuhi,
In a device with no VPU, when running the BSP the VPU is disable and if you run a video it will mark an error.
Regards
Hello Bio_TICFSL
Thank you for your quick response.
I hope to know which level it must care for no-VPU device.
Does it need a re-configuration for u-boot or Linux kernel?
Best regards,
Ishii.
No, you don´t need re-configured, Uboot detect which processor do you have, and the VPU is disable.