Add Include File From Outside of My Project[SOLVED]

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Add Include File From Outside of My Project[SOLVED]

3,697 Views
ramazan_kurban3
Contributor III

Hi. I want to  add include file from outside of my project. If ı add my inc folder to includes, builder give unreferance error. I cant add this folder to my project folder and ı cant create static library. How can ı add this folder to my project in MCUxpresso? 

SOLVED: 

WE MUST TO ADD SOURCE AND INCLUDE FILE TO "SOURCE LOCATION"

 pastedImage_1.png

0 Kudos
2 Replies

3,515 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Adding another folder with header files to the search path is really straight forward. Please take a look at the following screenshot.

pastedImage_1.png

Greetings,
MCUXpresso IDE Support

0 Kudos

3,515 Views
ramazan_kurban3
Contributor III

My settings is like this already. I think i need more setting. What do you think i'm missing ?

pastedImage_2.pngpastedImage_3.pngpastedImage_4.png

0 Kudos