Hi
I am reading the LPC546xx User Manual UM10912 Rev 2.4 11 November 2019 page 17. Here the memory map details can be found in the table 3 "Memory usage and details". The USB SRAM address range is given with: 0x4010 0000 - 0x4010 1FFC. Why is the upper limit terminated with a C and not with an F? (i.e. 0x4010 1FFF). Are the last three bytes in the USB SRAM reserved? Is this possibly a typo in the User Manual?
Dani
Hi Daniel Gull,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Why is the upper limit terminated with a C and not with an F?
-- I think it's a typo and its memory range should be 0x4010 0000 - 0x4010 1FFF (8 KB). In further, I'll report it to the document team for checking.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------