S32K144UFVLL FLEXIO_UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144UFVLL FLEXIO_UART

691 Views
729621187
Contributor I

When I use the flexio_uart of S32K144UFVLL,the data can't send out;but the same code running in demo board of S32K144UAVLL can send data.

0 Kudos
1 Reply

610 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello 729621187@qq.com,

What are the masksets of the two parts? 0N77P, ON74T, ON57U.
But based on the part numbers, both parts (S32K144UFVLL, S32K144UAVLL) support FlexIO and since it is working on the EVB, I reckon there is a HW issue.
Do you scope the pins?
Do you use SDK drivers?
If so, which version and what is the status returned by each function?

BR, Daniel

0 Kudos