Hi:
I have test 4.9.88 and 4.14.98 linux version and found the QT listwidget have some bug.When selecting an item of the list control, it does not disappear.
How to fix the issue?
Hello
They will, be added when qt jump to at least 5.13.2.
Regards
Do you think the issue is due to the Qt version?
I have done some test for it.
when using linuxfb to replace the wayland ,the list widget work well.
Compile the libqlinuxfb.so and copy it to /usr/lib/qt5/plugins/platforms
run the command 'systemctl stop weson'
and set the QT_QPA_PLATFORM
export QT_QPA_PLATFORM=linuxfb:fb=/dev/fb0:size=800x600:mmSize=800x600:offset=0x0:tty=/dev/tty1
after above process and run the qt demo,the issue solve.
But i still want to use wayland and weston.
Can you solve it on L4.9.14 or L4.9.88 version?