Hello,
About this doc in community
I use the patch that raw capture test and #include "g2d.h"
but when I build the program,it happened build error can not get g2d.h
what is the correct path?
Hello,
How to fix the patch build error?
Hi Xu
one can look at Software ISP Application Note
https://www.nxp.com/docs/en/application-note/AN12060.pdf
gtec-demo-framework/DemoApps/OpenCL/SoftISP at master · NXPmicro/gtec-demo-framework · GitHub
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I want to use the test application get Raw image,but now the code build error
Hi,
I said this imx8_ov5640_raw_captupre_test_4.14.98_2.0.0_ga.diff patch build error not softISP,
please help the build error