AnsweredAssumed Answered

temperature_monitor example

Question asked by Andy Dong on Dec 4, 2019
Latest reply on Dec 9, 2019 by Andy Dong

Hi,

 

I use imxrt1052 evkboard (SDK version 2.5.0)

I test the temperaturemonitor example but it's a little bit strange.

 

1. when the temperature is higher than DEMO_HIGHALARMTEMP(42U) 

    DEMO_TEMP_LOW_HIGH_IRQHandler() is triggered and then it will decrease the core frequency

2. when the temperature is lower than DEMO_LOWALARMTEMP(40U)

    DEMO_TEMP_LOW_HIGH_IRQHandler() is triggered and then it will change the core frequency to original.

 

I run the example. I use hairdryer to increase the temperature.

1. happened when the temperature is higher than 42. 

and then 2. didn't happened when the temperature is lower than 40.

 

Is there any suggestions ?

Thanks.

 

Best Regards,

Andy Dong

 

Outcomes